Part Number: TPD12S521
Other Parts Discussed in Thread: TPD1E05U06
Hi, I am using a SIL9022A with a TI TPD12S521.
Note the SIL9022A states it does not require a pull on CEC with IO voltages of 3.3v. I have the IO at 3.3v on the SIL9022A driven from an AM437x.
HDMI CTS 1.4b
VCEC2 is required to be in the range 0.196v to 0.274v with VCEC1 in the range 2.88 to 3.63v.
Using the TPD12S521 as defined in the DS 27k pull, series diode to 3.3v, on CEC at the HDMI connector. With a 47k pull on CEC at the
SIL9022A (controller side).
Diode MMSD103T1G.
VCEC2 is greater than 0.274v on two test samples, under the test criteria defined by CTS 1.4b. Slightly over. 0.277v & 0.279v. Must meet this spec including tol on 27k pull to 3.3.
CEC pulled with a 27k 5% resistor to 3.3v source, & 1k pull down on CEC.
What is TI take on this issue?
I know the AM437x evm uses a different clamp (parallel) with this encoder, was there a particular reason why?
Thanks
Barrie