This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AD: EEPROM programming without TIVA

Part Number: TPS65994AD


 In 994's EVM user guide, User can use TIVA to upgrade EEPROM data directly. But we have FTDI and Aardvark only. Where we can get TIVA debugger? How to update the EEPROM if i dont have TIVA

  • Hi,

    To update the EEPROM you could use the Aardvark and the Total Phase Flash Center application to load in the binary file which can be saved from the GUI Tool. Once you upload the low-region binary, you can connect with the Aardvark, select the EEPROM device, set the address (should be 0x50) and flash.

    Thank you,

    Hari