Part Number: PCA9548A
Dear team,
Could you please help to check what is the status of SCL and SDA of PCA9548A, ISO450/ISO451 when device is in power down mode or /reset pin pull low. Are they high impendence? Or pull-down? Thanks.
B.R.
Zhizhao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9548A
Dear team,
Could you please help to check what is the status of SCL and SDA of PCA9548A, ISO450/ISO451 when device is in power down mode or /reset pin pull low. Are they high impendence? Or pull-down? Thanks.
B.R.
Zhizhao
Hi Zhizhao,
I would like to point you to this post written by another Apps Engr Bobby. To summarize what he said:
t_w(L) is the time that the RESET pin has to be held low before the device recognizes a reset. So between 0s and t_w(L) the device does not recognize the reset so nothing will happen to the pins. Once the device recognizes the reset the SC0-7,SD0-7 pins will be deselected. This means that the FET that bridges the pins will become high impedance. This is the same for power down mode. When the device is powered off the pins are deselected.
Let me know if you have any further questions.
Best,
Chris