Part Number: DP83848VYB
Other Parts Discussed in Thread: DP83848I
Dear Technical Support Team,
My board has DP83848IVV / NOPB on mass production, but it is out of stock.
I'm confirming to replace from DP83848IVV / NOPB to DP83848VYB/NOPB.
I check two differences and these are temperature range and package (pin compatible but DP83848VYB has thermal pad).
There is no thermal pad pattern with DP83848I on my board.
■Question
①If the thermal pad is not used with DP83848VYB(LQFP), is the thermal resistance comparable to HLQFP?
Does it mean that operating temperature range will be -40 to + 85 ° C ?
② Do you have any other attention to replace ?
■temperature range
DP83848VYB/NOPB:-40℃~105℃
DP83848IVV/NOPB:-40℃~85℃

Best Regards,
ttd