Part Number: DP83867IS
Hi,
Customer has done experimentation DP83867IS as per Trouble shooting manual of TI -- snla246a. The details as below.
We have DP83867IS(SGMII mode) IC. to Marvell 88e630 Switch in SGMII mode its port 9. We are able to establish the link , but unable to exchange the Data with PHY IC.
- Ensured power supplies, RBIAS resistors,Magnetic Connections,Reset signal,Clock pins, We able to access resisters with PHY ID 0x09
- SGMII Lines are AC coupled with 0.1uF capacitor
- Worked on Far-end-Loopback mode and data is getting loop backed.
- Below are the Register values read through SMI interface.
0x0 -- 0x1140
0x1 -- 0x7949
0x2 -- 0x2000
0x3 -- 0xA231
0x4 -- 0x0181
0x5 -- 0xcc01
0x6 -- 0x006F
0x7 -- 0x2001
0x8 -- 0x6001
0x9 -- 0x0300
0xa -- 0x0800
0xb -- 0x0000
0xc -- 0x0000
0xd -- 0x0000
0xe -- 0x0000
0x10-- 0x5848
0x11 --0xB002
At marvell switch(88e6390) side we have verified the following.
- Using CRO we have verified that at power on switch is able to get data from PHY on SMI interface using PHY address '9'.
- Also we have verified switch(Marvell 88e6390) counters and there is no error when we analyze counters, i.e., all Ingress and egress counters on this port and the other port are matching always.
- PHY IC address is '9' and it is interfaced with 9th port of the Marvell Switch 88e86390.
- P9_SMODE pin tied pull-up -- SGMII mode
- Port status register0 -- bits 0:3 are configured as 0x0A for SGMII mode.
Regards,
Akshat
FAE