Hi Ti:
We're doing diag program. There are some error flags such as DPHY_ERROR in GENERAL_STS register and others. Which status need to be fixed manually? Can you provide some advise? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti:
We're doing diag program. There are some error flags such as DPHY_ERROR in GENERAL_STS register and others. Which status need to be fixed manually? Can you provide some advise? Thanks.
Hello,
What do you mean by "fixed manually"? Do you mean which bits in GENERAL_STS will need to be cleared manually? For example, DPHY_ERROR will not be cleared on read. In section 8.6.1.13 of the DS90UB941AS-Q1 datasheet the descriptions of each bit within GENERAL_STS are listed, and contain this information.
Regards,
Ben Dattilo
Hi Ben:
I mean, what are the real problems that need to be checked and corrected. Such as LINK_LOST error, if always exists ,need to check the equipments. I hope Ti can provide what status needs attention and inspection. Thanks.
BR,
Arvin
Hi Arvin,
What specific errors are you receiving? Each of the errors in the GENERAL_STS register should be addressed, however they may be caused by either software or hardware problems.
Regards,
Ben Dattilo
Hi Ben:
We're doing the diagnostic mechanism and want to know more info about important errors.
BR,
Arvin
Hi Ben:
This has nothing to do with this question. I just want to know what errors will affect the normal operation of the chip. Could you give some advice? Thanks.
Hi,
Apologies for the misunderstanding. All errors listed in the General_STS register (0xC) can affect the normal operation of the device and require attention. DSI_ERROR and DPHY_ERROR in bits 6 and 5 list several more specific errors that these general errors may represent. The more specific DSI and DPHY errors are described in the indirect registers.
Regards,
Ben