This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: WoL Power consumption

Part Number: DP83867IR


When the host is OFF and the LAN PHY is WoL, what is the lowest power consumption state and what is the mW?

Which is Deep Power Down, IEEE Power Down, Active Sleep, Passive Sleep?

If there are other chips with the following conditions that consume less WoL, please introduce them. I would like about 25mW.
-GbE
-Host side I / F: RGMII 1.8V