Part Number: DP83869HM
Other Parts Discussed in Thread: USB-2-MDIO, DP83869EVM
We're using DP83869HM for application RGMII to 1000Base-X, SFP Fiber with Default Register Configuration (by strap pin) and try to set up a proper configuration via MDIO.
In parallel we tried with DP83869EVM different MDIO Configuration to set up the communication using USB-2-MDIO Tool. Link up with SFP gets identified but no RGMII communication at all.
MAC - DP83869HM - SFP Fiber Module
Output Register Readout:
Register 0000 is: 1140
Register 0001 is: 6169
Register 0002 is: 2000
Register 0003 is: A0F1
Register 0004 is: 0020
Register 0005 is: 41A0
Register 0006 is: 0007
Register 0007 is: 2001
Register 0008 is: 0000
Register 0009 is: 1300
Register 000A is: 0000
Register 000D is: 401F
Register 000E is: 0000
Register 000F is: F000
Register 0010 is: 5448
Register 0011 is: AC02
Register 0012 is: 0000
Register 0013 is: 0444
Register 0014 is: 29C7
Register 0015 is: 0000
Register 0016 is: 0000
Register 0017 is: 0040
Register 0018 is: 6150
Register 0019 is: 4444
Register 001A is: 0002
Register 001E is: 0012
Register 001F is: 0000
Register 0025 is: 0480
Register 002C is: 141F
Register 002D is: 0000
Register 002E is: 0221
Register 0031 is: 10B0
Register 0032 is: 40D0
Register 0033 is: 0000
Register 0037 is: 0003
Register 0039 is: 0000
Register 003A is: 0000
Register 0043 is: 07A0
Register 004F is: 0166
Register 006E is: 0200
Register 0086 is: 01D3
Register 0134 is: 1000
Register 0135 is: 0000
Register 0170 is: 0C0F
Register 0180 is: 0752
Register 0181 is: C850
Register 0182 is: 5326
Register 0183 is: A01E
Register 0184 is: E976
Register 0185 is: 19CF
Register 0190 is: 0000
Register 0191 is: 0000
Register 0192 is: 0000
Register 0193 is: 0000
Register 0194 is: 0000
Register 0195 is: 0000
Register 0196 is: 0000
Register 0197 is: 0000
Register 0198 is: 0000
Register 0199 is: 0000
Register 01A4 is: 0000
Register 01A5 is: 0000
Register 01A6 is: 0000
Register 01DF is: 0041
Register 01E0 is: 417A
Register 0C00 is: 1140
Register 0C01 is: 616D
Register 0C02 is: 2000
Register 0C03 is: A0F1
Register 0C04 is: 0020
Register 0C05 is: 41A0
Register 0c06 is: 0005
Register 0c07 is: 2001
Register 0c08 is: 0000
Register 0c18 is: 01FF
Register 0C19 is: 0031
As a result of some tests, a proper workaround to enable communication is to set Register 0x86 to 01XX except 00XX.
Whats the the behaviour of DLL_EN_FORCE_CTRL and what does it affect?
The other CTRL Bits doens't have an affect.
Are there any other register needs to be set, for proper RGMII Configuration?