Part Number: TUSB8020B
Hi,
We use open source USB 3.0 hub schematic based on TUSB8020B. When we tested the board USB 2.0 part has successfully detected by the PC and works. But USB 3.0 part of the device does not work and is not detected by the UsbTreeView software.
1. Upstream connected to PC USB2.0 port:
- current consumption: ~ 80 mA;
- board detected in USBTreeView as USB2.0 hub;
- board works correct and doesn't heating;
- signal on TX line presents below.


2. Upstream connected to PC USB3.0 port (has been checked usb3.0 function):
- current consumption: ~ 260 mA;
- board detected in USBTreeView as USB2.0 hub;
- board works correct as USB2.0 hub and heating over 60C;
- signal on TX line not stable. Variations presents below.


We've read topic where Justin Y describe similar problem and then checked thermal pad connection of our board by X-ray. It was uncertain and we made new board with good thermal pad contact (X-ray checked too), but behavior was the same with the first board.
We used the shortest cable we have, checked two samples of board and two different PCs. What else should we do to make USB 3.0 part of the device work.
We would greatly appreciate your help in creating this design.