This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: For configure the Registers

Part Number: TPS25750

Hi,

Right now, i am going on the step to configure the Registers. For it's first time for me to configuring the PD controller, so there are some simple questions? Sorry.

The following blank:

- Could the R/W registers be configured only? Users cann't configure the RO register when configure the PD controller, only allow to read, right?

- What is the 4CC Task? when to use the 4CC commands? The 4CC commands will not be used when configure the registers, right?

The 4CC commands are used for if when users want to get some information or to load a Patch Bundle, then send these 4CC commands to PD controller, Right?