About DS90UB941 Splitter mode: 2*H = 3840, V = 1080 or H = 1920, 2*V = 2160 is input, can the resolution of both output images be configurable to 1920*1080@30Hz?
Importantly, we want two outputs with a resolution of 1920*1080@30Hz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
About DS90UB941 Splitter mode: 2*H = 3840, V = 1080 or H = 1920, 2*V = 2160 is input, can the resolution of both output images be configurable to 1920*1080@30Hz?
Importantly, we want two outputs with a resolution of 1920*1080@30Hz.
Hello Kijung,
Only the bottom picture is supported by 941AS. So the 2xH = 3840, V = 1080 can be split to 2x 1920x1080@30
Best Regards,
Casey