Part Number: ONET4201LD
Other Parts Discussed in Thread: DSLVDS1001
According to the datasheet of ONET4201LD, DIN+/DIN- are CML-IN.
However, the output of FPGA is COMS.
Therefore, I need a converter, which can convert CMOS to CML-IN.
Would you please suggest one?
Thanks a lot.
Besides, the speed of DIN+/DIN- is almost 200MHz.