Part Number: SN65C3223
Hi Team,
will the device work as expected if Pin 14 is not connected. My customer wants to replace a Exar device (
SP3222EBEY-L).

Thanks
Jan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jan,
This is an older device, so it doesn't have an internal pull-up or pull-down to set the state of the FORCEON pin. Thank being said, leaving it floating will put it at GND in most cases, which enables the Auto Powerdown feature. This feature disables the RS232 driver outputs if no valid RS232 signal is detected. So the device will work, but that feature will be enabled if FORCEON is at GND level.
Regards,
Eric Hackett
Hi Eric,
does it mean if my customer just replaces the devices without modifying the layout, that some devices will work and others not?
will put it at GND in most cases,
Best regards
Jan