Part Number: PCA9539
Hi, I ask to review the circuit diagram about PCA9539.
PCA9539 Ref. Des : U72, 73, 74
I will be waiting for the reply.
Thank you !!Connect_RG_20210826.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9539
Hi, I ask to review the circuit diagram about PCA9539.
PCA9539 Ref. Des : U72, 73, 74
I will be waiting for the reply.
Thank you !!Connect_RG_20210826.pdf
| PCA9539 (U72, U73, U74) | ||
| Checked: | Status: (Good, Bad, Okay, ?) | Comments: |
| Schematic pinout matches datasheet | Good | |
| Decoupling Cap on Vcc | ? | Decoupling Cap is missing |
| SCL/SDA on schematic pin out matches SDA/SCL net name | Good | |
| RESET biased correctly | ? | Verify that RESET is not being over biased above Vcc logic. Refer to 8.2.1.1 RESET Errata |
| Unique Addresses between the other IO expanders | Good | |
| P-Ports are properly Biased | ? | U74 pins 17-20 are floating, this can be okay if device is programed to have pins set to an output, if left an input then you need to bias the pin to either GND or Vcc with a resistor. (otherwise shoot through current and higher supply current) |
-Bobby