Part Number: THVD1550
Hi Team,
Our THVD1550 have Integrated IEC 61000-4-2 ESD protection(18kV). Does it means customer don't need any external protection(such as TVS or ESD protector) for IEC 61000-4-2 ESD test?
BR,
Victor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1550
Hi Team,
Our THVD1550 have Integrated IEC 61000-4-2 ESD protection(18kV). Does it means customer don't need any external protection(such as TVS or ESD protector) for IEC 61000-4-2 ESD test?
BR,
Victor
Hi Victor,
Yes. The listed rating shows that this device can pass IEC 61000-4-2 ESD testing at the listed levels without any external protection. If higher levels are required by the final design, external protection may be added to increase system resilience.
Let me know if you have any more questions.
Regards,
Eric Schott