Part Number: DS90UB953-Q1
Hi there
I'm a South Korean Automotive camera engineer.
Please review the DS90UB953-Q1 circuit.
We are planning to use Non Sync Mode. Therefore, an external oscillator was added.
10k and 4.7k were adopted as Strap Configuration Mode resistance, and 5% resistance will be used.
I added a table below that calculates the mode pin input voltage using 10k and 4.7k.
| Max | 0.615 |
| Typ | 0.576 |
| min | 0.537 |
And, I didn't add ferrite beads to the poc line, should I?
Additionally, we use MIPI 4 Lane.
Please refer to the attached circuit as well.

Thank You!