This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83620: overshoot and undershoot

Genius 14490 points

Part Number: DP83620

Hi team

I need the overshoot and undershoot values for DP83620SQ/NOPB 's clock connected at X1 pin

also can you give me the VIH (max) and VIL(min)??


Best regards,
William

  • Hi William,

    The overshoot/undershoot values are located on Table 4.2 of the datasheet. Depending on the supply voltage, you will either have a +/- 10% or 5% wiggle room.

    Regarding VIH and VIL, there is no VIH max or VIL min as these are the thresholds where the PHY recognizes a signal as high or low. To recognize a high, the signal must be above 2V, but should not exceed the I/O supply voltage. To recognize a low, the signal must be below 0.8 (3.3V I/O supply) or 0.7 (2.5 I/O supply) and should not be lower than GND.

    Sincerely,

    Gerome

    All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and it is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).