Part Number: DP83867IR
May I have a question for Pin requirement of DP83867IR
Question1.How much load capacity is acceptable at Vosc pin?
Connectable *pF
Question2.Electrical Characteristics of Vosc
There is described "XI INPUT VOLTAGE" that is Min1.5 Max1.9 Vpp in Datasheet.
This mean is Peak to Peak voltage requirement and There is no requirement of Low level in Datasheet.
Does it work with Low level signal is under -200mV?
Question3. Supply voltage for VDD1P1 (PAP) Min1.045-Max1.155 and VDD1P0 (RGZ) Min0.95-Max1.155 in Data Sheet
How much high frequency could we ignored or filltered for these power when we measure it with ociloscope?
Could we ignre 20MHz over?
Regards,
Kosaka