Part Number: SN65HVD888
Hi engineers,
I'm recommending SN65HVD888 to customers and there are some technical details that need your help to confirm.
As we know, SN65HVD888 equipped with polarity correction function which need pull up resistor to ensure high voltage level when Bus IDLE As directed by A datasheet .

Background:
1.The equipment developed by the customer belongs to 485 slave, the pull up resistor in master side is uncertain, so whether the polarity correction function cant work is uncertain.
2.The communication standard adopted by the customer is MODBUS, I don't know much about MODBUS, he said that in the Modbus protocol, each device can be either a master or a slave.
question:
I want to put pull-up resistor at customer's equipment side(slave node) , maybe it can ensure high voltage level when Bus IDLE and ensure polarity correction function can work?
If it works, there are any risks during it? such as too much pull-up resistor decrease number of nodes that can be connected to the bus.