Part Number: TSER953
Other Parts Discussed in Thread: TDES954
We have a TSER953/TDES954 link and some times we are able to get some number of frames over the link. However, more often than not, on initialization we are getting the following CSI errors.
FPD 953 Reg 0x5C - CSI Err Count : 02 FPD 953 Reg 0x5D - CHKSUM / ECC Err : 00 FPD 953 Reg 0x5E - LANE01 Err : 46 FPD 953 Reg 0x5F - LANE23 Err: 64
Several questions:
1. Those errors correspond to "Multi-bit error in SYNC sequence - Uncorrectable" and "Control Error in HS Request Mode". What do those mean? Can we do anything about them?
2. Those errors are making it so the LOCK/PASS link gets dropped and then no further frames can be obtained. Is there a way to make it so that errors don't cause a drop in the link?
Thanks,
luis