Part Number: THVD1500
Hi,
Since the chip has ESD protection inherently, do we need to add external TVS diodes?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1500
Hi,
Since the chip has ESD protection inherently, do we need to add external TVS diodes?
Hi,
Thanks for the reply.
If we are okay with the ESD ratings of the IC, should we add clamping current limiting pulse proof resistors?
Akash,
As Clemens said, if you are concerned about ESD events stronger than what the device is rated for, it is recommended to add external protection components. TVS diodes and/or current-limiting pulse-proof resistors are both good options.
Regards,
Eric Hackett