Does the INT pin of DP83TG720R have to be used? I know that WAKE and INH pins can be not used if I don't need these functions. I wonder if INT can be not used.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does the INT pin of DP83TG720R have to be used? I know that WAKE and INH pins can be not used if I don't need these functions. I wonder if INT can be not used.
Thanks.
INT pin is output of the PHY. So it is upto the user to use it or not.
--
Regards,
Vikram
Hello Hui,
INT is not an RGMII signal and Rgmii can be used without INT.
--
Regards,
Vikram