Part Number: TS3USB3200
Other Parts Discussed in Thread: TMUX136, TS3DDR4000, HD3SS3412, TS3DV642, DS42MB200
H Team,
Our customer is looking for a VBO-HS splitter to distribute the signal into 2 outputs. According to our customer,
VBO-HS maximum frequency is 4 GHz. I have 8-lanes (8 differential pairs). So I would need 8 ICs (if the IC is SPDT). I highly prefer a distributor IC which splits the signal but a switch is also welcome. I thought of TMUX136, what do you think? I only need to deal with 2 lanes, while the other 6 lanes are going to only one direction. therefore, due to skew issues and inter-skew stuff I thought that using 8 ICs is best to have similar skew between all lanes.
He is considering TS3USB3200RSVR but it's currently out of stocks. Is TS3DDR4000 suitable for this application? If not, do we have other device that fits his requirements which has stocks?
Regards,
Danilo