Hi,
The datasheet describes the following explanation of max SPI rate in P.32.
"If VIO is present in sleep mode, SPI access can take place but at a reduced rate. If at least a 10 μs delay is used between pulling nCS low and the start of a read or write the max SPI rate can be utilized."
Q1) Is the max SPI rate 10kHz here?
Q2) Why the 10 us delay is required for max SPI rate then?
Best Regards, Taki