Part Number: DP83867E
Good morning,
What is the drive strength of the RGMII transmit signals of the PHY? Is it also configurable?
Best Regards
Onur
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867E
Good morning,
What is the drive strength of the RGMII transmit signals of the PHY? Is it also configurable?
Best Regards
Onur
Hello Onur Kusakoglu
Thank you for the query.
he driver strength i not configurable. The interface can connect to a MAC with 4 to 6 inches of trace length.
Can you please explain the use case and the need to know the drive strength.
Regards,
Hello Onur Kusakoglu
Thank you for the query.
The drive strength is not configurable. The interface can connect to a MAC with 4 to 6 inches of trace length.
Can you please explain the use case and the need to know the drive strength.
Regards,
Sreenivasa
I have placed some series resistors and want to understand the power dissipation on these resistors. This is why I want to understand the drive strength of the PHYs. My traces are no longer than 2.5 inches.
Hello Onur Kusakoglu
Thank you for the reply and information.
We support interface length between 4-6 inchs and so 2.5 inch should not be a concern.
We do have impedance control that you can use. Other than the link provided above do not have a number that i can provide.
Regards,
Sreenivasa
Hello Onur Kusakoglu
Thank you for the reply.
If you do not have additional questions, please click the resolved button to close the thread.
Regards,
Sreenivasa