Part Number: TPS65988
Hello,
Can I get the TPS65988 EVM out of the box default configuration file(project) in .pjt format. We are using TPS65988 PD controller in one of our designs and we are testing it with the EVM.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65988
Hello,
Can I get the TPS65988 EVM out of the box default configuration file(project) in .pjt format. We are using TPS65988 PD controller in one of our designs and we are testing it with the EVM.
Anushree,
When you load the GUI, If you create a new project, select the TPS65988 as the device, select the advanced option, then select the Dual Role Port (DRP), prefers power source.
This will create a project that is the same configuration as the default EVM. The only difference that you will see is that the version of firmware used will be the version of firmware provided with the GUI, rather than the version used when the EVM was manufactured. They may be different.
Regards,
Chuck