Part Number: DP83822I
Other Parts Discussed in Thread: DP83TD510E,
Hi Team,
We are developing a SPE(DP83TD510E) to 10Base-TE(DP83822i) media convertor.
For MDI side on DP83822i we are using capacitive coupling (not magnetics).
Is it necessary to write the following register for 10Base-Te operation?
- Line Driver Class Selection Register<0x0404> = 0x0024 To program full MLT-3 on both Tx+ and Tx– (Class A)
Or is this only required when operating PHY with Capacitive Coupling at 100Mbs?
I have referenced the following forum link for the above register write;
Our design will sit on a backplane and PCB trace distance from PHY-PHY is ~100mm.
Kind Regards,
Daniel