Part Number: DS100BR210
My requirement is to connect the RJ45 interface of a PC to a network switch with a redriver unit between them. I tried using DS100BR210 but realised that it works only with 10G-KR. Is there any similar IC available which works for Base-T? I would like something which works for 100 Base-T (MLT-3 encoding) as well as 1000 Base-T (PAM-5) since I'll be using both.