Part Number: DS100BR210
Hello,
We are using the DS100BR210 in 10G-KR Mode. (Back-plane)
It is configured as follows:
ENSMB = 0 (Pin Mode)
VOD_SEL = 1 (10G-KR Mode)
VDD_SEL = 0 (3.3V Operation)
MODE = 1 (10GbE Mode, Continuous Talk)
TX_DIS = 0 (OUTA and OUTB Enabled)
SD_TH = Float (180 mVpp, 110 mVpp (Default)
Since this is a 10G-KR mode with auto negotiation what logic level should the following be tied to?
EQA1,EQA0
EQB1,EQB0
DEMA, DEMB
Can they be let floating?
THANKS
Jeff