Other Parts Discussed in Thread: DP83869
Hi, I used DP83860 as a 1000M media-converter. But there's datagrams loss at a rate about 0.02%. It seems that FIFO overflow. I configured PHY_CONTROL to 0xF048), that FIFO Depth is 4 Bytes. But there's still packet loss. Is this register configured correctly?
And should the value of RX_ERR_CNT register(Address 0x15) be non-zero if there's packet error? I found the value of RX_ERR_CNT register was zero when there's packet loss.
Thanks!