Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869, DP83869EVM,
Howdy All,
I have a few questions about what Aniruddha Khadye previously stated in https://e2e.ti.com/support/interface/f/138/t/791559?tisearch=e2e-sitesearch&keymatch=DP83869HM%2525252520managed%2525252520media%2525252520converter:
1.) "DP83869 needs software access to work in media convertor mode. The software setting is mentioned in the datasheet."
a.) Is this the datasheet statement: "When Media Convertor Mode is enabled then bit [0] of register 0x01EC should be set to 0."?
b.) And if so, what does this bit actually do and why is it needed?
2.) "Also the speed needs to be same on both the copper and the fiber side. The Copper side can auto-negotiate down between 1000M and 100M but the fiber ethernet standard does not support auto-negotiation. So the Fiber speed would need to be changed by software between 1000M and 100M."
a.) If this is so, then why do we have end to end Ethernet communications with the following setup?
100M Copper <> Eval Board #1 (DP83869EVM with strap config only) <> 1000M Fiber SFP <> Fiber Cable <> 1000M Fiber SFP <> Eval Board #2 (DP83869EVM with strap config only) <> 100M Copper
b.) What register needs to be changed in software to configure the Fiber speed to 100M?
Regards,
Dan