Part Number: MAX3227
Other Parts Discussed in Thread: MAX3221
Dear,
as below , the picture 1 is max3221 function table , and picture 2 marked is max3227 function table , but max3227 input conditions there is receiver or driver edge within 30s status, can you help me understand the difference between max3221 and max 3227,now i use max3221, whether to use max3221 directly instead of max3221 ?
picture 1.

picture 2.