This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
as below , the picture 1 is max3221 function table , and picture 2 marked is max3227 function table , but max3227 input conditions there is receiver or driver edge within 30s status, can you help me understand the difference between max3221 and max 3227,now i use max3221, whether to use max3221 directly instead of max3221 ?
picture 1.
picture 2.