This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
my purpose is to connect the 100 ohm differential output of the phy chip to LMH0302, LMH0001 or others, so as to achieve IP network transmission over a single coaxial cable. I wonder if this is possible? Do you have any relevant suggestions? I am attaching a schematic.The phy chip I use is DP83TC811 or other
Hi Zhang,
As long as you have NRZ data within the LMH0302 data rate limitation you should be able to use these drivers. These are protocol agnostic. You can consider DS30BA101 targeted mainly for these types of applications. Here is a link to this part's data sheet:
Regards ,, Nasser
Thank you so much for your reply, I have sent you a friendship request. I've checked out the DS30BA101, and once again the LMH0302, I'll go into more detail later.
Hi Zeshan,
I just responded to your message. Please let's discuss this through your friend request.
Regards,, Nasser