Part Number: MAX3243E
Other Parts Discussed in Thread: MAX3243
Hello guys,
One of my customers is evaluating MAX3243E which has auto-powerdown mode for their new products.
Their loop-back test (shorted RIN5(No.8 pin) to DOUT3(No.11)) was failed when the auto-powerdown mode is enabled (FORCEON=L, /FORCEOFF=H).
And the loop-back test was passed when the auto-powerdown mode is disabled with /FORCEOFF=L.
The related E2E thread
says that "With loopback, this problem cannot happen. TX_OUT will output a valid signal for at least 30 µs, which will keep the transceiver out of powerdown mode."
I think this mean is that MAX3243E doesn't go into the auto-powerdown mode as long as RIN is shorted to DOUT before MAX3243E is powered up.
Is my understood correct?
Also do you have any idea why did their loop-back test was failed when the auto-powerdown mode is enabled?
Your reply would be much appreciated.
Best regards,
Kazuya.