Part Number: DS90UB935-Q1
Dear expert,
Customer system is SoC+UB962+UB935+Slave. SoC is I2C master.
SoC need to read continuous 3072 bytes from Slave through I2C. In real vehicle test, occasionally, SoC can only read the first for example 1000 bytes(randomly) correctly and following bytes are all 0xFF. There is no any I2C error reported. Customer measured I2C signal with I2C protocol analyzer at both UB962 side and UB935 side.
At UB962 with SoC side, SoC issued 3072 bytes read and UB962 return 0xFF after first 1000 bytes with I2C protocol analyzer.
At UB935 and Slave side, UB935 only issued 1000 bytes read with I2C protocol analyzer capture. Then there is no any I2C traffic recognized by I2C protocol analyzer. No error is reported as well.
Could you give me any help on this? What might cause this?