Part Number: TPS25750
Other Parts Discussed in Thread: BQ25792, , USB-PD-CHG-EVM-01, BQ40Z50
Hi Chuck,
Some follow-up questions based on my previous thread:
1) Will the TPS change its RX_SINK_CAPS and TX_SOURCE_CAPS registers during operation? (I.e., do I have to read and then write to change the numValidPDOs, or could I just write based on a known configuration?)
2) The BQ25792 can handle faults of the battery either not wanting to discharge (empty) or not wanting to charge (full). Could you elaborate a little more on how this plays out? For example:
a) Does the TPS25750 learn what is going on and communicate this over USB-C to the attached device?
b) If the battery is later available, will the TPS or BQ figure this out and start charging/discharging, or would this require some other action? (Like unplugging and re-plugging in, or the micro sending a command to the TPS or BQ vis the TPS)
3) Did you create a post discussing TPS/BQ command interface/pass-through commands? (last post in the previous thread)
Thanks,
-Eric