This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: LOCK lost EMC test

Part Number: DS90UB948-Q1

Hello,

we have the same problems as descibed in the related question.

Is there any further information on the issue in the meantime?

The lock loss problem occurs between 600MHz and 1000MHz.

Thanks & Best Regards,

Tobi

  • Hi Tobias,

    As far as I remember, we do not have any issue getting 948 to pass EMC. Can you tell me which test you failed due to the lost of lock RI, RE, BCI? Can you share the EMC testing results?

    Aaron

  • Hi Aaron,

    this was the test:  Radiated Susceptibility - disturbing field 100V/m CW

    We started at 200MHz and from 600MHz onwards there were the described losses of lock.

    Tobi

  • Hi Tobias,

    The 948 doesn't have external input reference clock. It uses the PCLK to generate the desired the frequency. If it's in dual link then the frequency is too low. If it is dual link, it has to be a minimum of 50MHz. When I used the frequency you provided and divided it the encoding of 600MHz/35=17MHz; 1000MHz/35=28.5MHz. It doesn't meet the minimum input clock requirement.

    Aaron