Part Number: PCA9306
Other Parts Discussed in Thread: SN74LVC2G66
Hi,
if I connect VREF1 and VREF2 both to 3.3V, and I don't need the voltage translator function.
Can I use it as I2C buffer? When enabled, side 1 and side 2 are connected together, when disabled, side 1 and side 2 are not connected together.
If it can be used as I2C buffer, can I use it to replace TCA9511 if I don't need READY signal?