Part Number: TUSB212
Other Parts Discussed in Thread: TUSB216-Q1
Hi Malik Barton57,
Thanks for the response. Can you please confirm what is the Maximum Pre channel and Post channel length supported by this TUSB212 Redriver .
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB212
Other Parts Discussed in Thread: TUSB216-Q1
Hi Malik Barton57,
Thanks for the response. Can you please confirm what is the Maximum Pre channel and Post channel length supported by this TUSB212 Redriver .
Thanks
Hi,
You can use this table as a reference.

Thanks
David
Hi David.
Thanks for the response. Can you please share Maximum Pre channel and Post channel length supported by this TUSB212 Redriver in inches for Layout design.
We are using Type4 (2-6-2+) stackup with EM390 material. Thickness of board is 0.7mm.
Thank you
Hi,
Due to the nature of our USB 2 redriver solution there is no specific insertion loss (in dB) that accurately corresponds to a particular boost setting of the device. Please find the rough estimates below for AC boost provided by TUSB216-Q1. These numbers are based on eye diagrams in the datasheet and are all typical values.
AC Boost at 240MHz (typ)
Boost 0: 3.0 dB
Boost 1: 3.5 dB
Boost 2: 4.7 dB
Boost 3: 5.2 dB
You can also used the cable length in the app note I sent as a reference.
Thanks
David