This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: cable effect

Part Number: DS90UB960-Q1

Hello,

One customer used 953/960 for his application as below, he used two cable which connected with a connector. The lengh of cable 1 is about 0.3m and the cable 2 is about 2m.

The problem he met is that sometimes the image didn't fresh and jammed. 

If he shaked the connector between cable1 and cable2 slightly, the video picture will jam, and then stop shaking, and then it will start to display normally. Read the 0xD3 register for the TI 960 and notice that its value is always  changed. The change is shown (each point in the figure is converted to a specific level of EQ based on the value 0xD3)

Sometimes if he disconnected the cable 1 and cable 2 , and connected again, it would display normally again.

Could you please help to analyze?

Best regards

kailyn