Part Number: P82B715
Other Parts Discussed in Thread: LM1117
Hello,
There seems to be conflicting information on the TI website regarding I2C pullup resistors.
I2C Bus Pullup Resistor Calculation (2015)
https://www.ti.com/lit/an/slva689/slva689.pdf
P82B715 I2C Bus Extender (2016)
https://www.ti.com/lit/ds/symlink/p82b715.pdf
The example in the first link on page 4 suggests values from 1 to 2 K.
However page 12 in the datasheet shows values much higher. Is that specific to the P82B715 or have opinions changed on the recommendations?
The circuit is 5V powered. Mcu is ESP8266 (ESP-01), supplied by a LM1117 to drop to 3.3V. The local I2C devices are powered by 5V with the SDA and SCL lines pulled up to 3.3V. Lx and Ly are pulled up to 5V, as well as the remote SDA and SCL.
Thanks all for your insight.
Mark.