Part Number: DS90UB940-Q1
hi Logan
If the DS90UB940-Q1chip is used normally, do I need to initialize its registers? If so, which registers need to be initialized
regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB940-Q1
hi Logan
If the DS90UB940-Q1chip is used normally, do I need to initialize its registers? If so, which registers need to be initialized
regards
Hi Jie,
This is highly dependent on application/use-case, but at a high level these 94x DES devices need very little register configuration for operation.
Do you have a specific feature/function your curious about implementing?
Regards,
Logan
Hi Jie,
If all mode straps are correct for your desired CSI configuration then no registers need set.
Some general registers that you can use for reference to verify settings and configure are the following. Information on these are in the datasheet.
Regards,
Logan