Part Number: DS26LV31T
Other Parts Discussed in Thread: STRIKE, THVD1449V, THVD1449, THVD1428, THVD1429
Hi.
I have to protect against lightning and interferences a telemetry line RS422 which uses a DS26LV31T as driver. Therefore I would like a model of the three state Output Buffer to carry out Spice Simulations attacking the driver output with waveforms about 250 V and 10 A:
1- I have tried the Ibis model but the results don´t convince me because it doesn’t include the ESD clamping diodes. I´ve developed a model by advice of other designers that you can see in file Capture1, do you think is a proper model for the outputs, let´s say pins 2 &3? Can you provide me a model of the output driver impedance?
2- Could you tell me the output impedance when the driver is in high impedance and in normal operation? (I mean, an average).
3-I don´t understand the maximum rating of the Driver Output Voltage, it´s written in the datasheet (Power Off:D0+, D0-), what is the meaning of (Power Off:D0+, D0-)? Is differential, single ended or what? Is the same maximum rating when the device is powered at 3.3 V.
4-Last but not least, I have to apply waveforms that are mainly pulses or damped sinusoids, if the maximum ratings are exceed for a time let´s say 30 uS, how I could asses if the driver has survived the lightning/ interference? (See pdf file attached) .