This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86:How to setup with 4K2K DP monitor

Other Parts Discussed in Thread: SN65DSI86

Use DSIA and DSIB Dual DSI?

Here's my understanding, i need to confirm.

SOC should divided 4k2k signal into odd and even and transmitted with 2 DSI(soc) (4 Lane *2) , then connecnt DSIA and DSIB, is right?

even SOC 's 1 Lane  can transfer 1.66Gbps

Other question 2:

1.because 4K2K monitor's EDID of pixel clock is 533Mhz, it is over calc tool to use.

So how can i do? if i want to support this 4k2k monitor (Pixel clock is 533Mhz).

Please help  explain with SOC and HW BLOCK_DIAGRAM, thank you

2. SOC DSI Data rate is 1.66Gbps  over SN65DSI86 1.5Gbps. What will happen? Soc need to down data rate?