Part Number: DS90UB960-Q1
Hello,
As the below post said: the 960, 953, and 933 all need to be set to the same RAW mode in order to run simultaneously in one setup. And when RAW mode data is received by the deserializer, it is then converted to CSI-2 Tx packets with assigned data type and virtual channel ID.
So I'd like to confirm if four 953&935 connected DS90UB960 and they set to RAW mode, for example, do the four input set the same RAW10 or RAW12? If it is feasible with three RAW10 and one is RAW12 ?
And if the 953&935 configured the CSI-2 mode, and the four input should be the same data type? If it support that one is YUV422 8bit and others are YUV10bit ?
Best regards
Kailyn