Other Parts Discussed in Thread: BQ25895, TPS25750, TPS25810
Hi,
I posted in the power management forum and got some ideas. Basically we have a USB 2.0 pass through board that has some power management on it (charger, power path control to a touch controller downstream, and bluetooth module that communicates with touchcontroller). We'd like to be able to charge at 15W using USB-C, but also be able to fall back to the next highest charge rates if USB-C is not detected (e.g. USB-3.0 dedicated charge port 7.5W). Our block diagram currently looks like this:

The thinking was to use pull-up resistors to negotiate USB-C power (3A if possible) and have the BLE module read the voltages at CC1/2 to ensure the BQ25895 matches its charging current appropriately. But I'm wondering if this is too simple a solution and maybe you have a USB-C controller that is more appropriate? Like the TPS25750? Thanks for any advice you have.
Erik