Part Number: TCAN4550
Hi,
We are using TCAN4550 module in i.MX8M Mini processor-based hardware with modified tcan4x5x driver of kernel 5.4.70.
1. I need to set the TCAN4550 module to sleep mode when not in operation and set to normal mode during send/receive operation. Is it possible to achieve this in the driver, if so could you tell me the sequence and which register has to set.
2. Whether it is possible to make CAN as wakeup resource. Set the entire system/hardware in sleep state and with CAN interrupt the system/hardware wake up.
Regards,
Deeksha