Part Number: TPS25772Q1EVM
Hello,
I am asking a related question towards I2C commands sent to the TPS2257 module. On the USB-PD GUI that is used to configure settings, there are I2C Slave Addresses: (0x22 for Port A and 0x26 for Port B) that can be read to determine the output voltage. Port A seems to have more information and even displays the DCDC1 VCode and DCDC1 Current Code. I am planning to hook up a Raspberry Pi to these I2C lines and reading these values back would be a great way to confirm that my system is working properly. Is there any software interface sheet that has the I2C commands on the slave address to read these values? Thanks again...