Part Number: TLK2711-SP
Hi, everyone.

This is the maximum jitter value as defined in the datasheet of TLK2711-SP.
Is it total jitter or TIE?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK2711-SP
Hi, everyone.

This is the maximum jitter value as defined in the datasheet of TLK2711-SP.
Is it total jitter or TIE?
Hi,
This is total jitter.
Thanks,
Drew
I measured the jitter of txclk.
Should the value of the red square box in the picture be less than 40ps?
What is the meaning of tj max, min of the blue box in the picture?

Hi,
I would probably rely more on the min/max since those seem better correlated with the mean and std deviation. Do you know what probability level was used for this measurement? It seems strange that peak-peak is less than min/max.
Thanks,
Drew
Please refer to the below figure.

Is the maximum jitter generated 498.72ps?
Should I compare the 40ps specified in the datasheet with maximum jitter value of the measured Tj?
Hi Dean,
Given that it's not clear how p-p is measured on this equipment, I would refer to max jitter.
If you are measuring the clock output from the RTG4 PLL (linking other thread for future reference), I think this is consistent with the datasheet from that part. Jitter is expected to be 2% * (1/fin) + (1.45 * Input Jitter). I'm not sure what your input jitter is, but 0.02*(1/50E6) = 400ps, which is somewhere around 498ps that you measured.
Thanks,
Drew
Hi Drew.
I don't understand the meaning of peak to peak of total jitter(Tj). Total jitter has a mean, maximum and minimum value.
Isn't peak to peak period jitter or TIE?
I will try to measure it again.
Please tell me how to set up the oscilloscope for measuring TXCLK.
1. If the FPGA bypasses the clock, can I set the recovery clock as a constant clock?
2. Can I set the BER 1E12?
3. How do I set up HPF or LPF?
Thank you for all your assistance.
Hi Dean,
I am looking into this and will get back to you with more details tomorrow.
Thanks,
Drew
Hi Dean,
Apologies for the delay. I am working on getting advice from a teammate who is more knowledgeable about clock jitter measurements. I should have an update early next week.
Thanks,
Drew